hi all
we are designing a stepper motor controller, using DRV8824
my question is is it possible to change the direction on the fly?
what all should take care / procedure to do so?
secondly how should we define which decay mode is to be used?
how much time will the motor be on hold condition after the drive is enabled?
what defines the motor supply voltage?
the motor supply voltage(VM) is ranged from 8V - 45V and maximum drive current is shown as 1.6A at 24V
so, how can we calculate the drive current in different voltage levels?
regards
sunish