I need a dual stepper driver like the DRV8821/23. The DVM appear to be based on MSP430 but there is a “Control Suite” and Digital Motor Control (DMC) Libraries that is based on the DSP320C2000. The DMC appears to have significant software function to speed firmware development.
Questions:
Is the “Control Suite” or DMC applicable to the MSP430 based DVM? (C code that can be ported from 32-bit to a 16-bit MSP430?)
Is there a DRV8821 Dev Kit for the C2000 launch pad?
Are there examples of encoder used with the MSP430 and DRV8821/23?
Since I plan to use two Steppers but can not rule out a DC motor, is there a downside to starting with a DRV8823 rather than the Stepper only DRV8821?
LDT