This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Full step mode using DRV8811

Other Parts Discussed in Thread: DRV8811

We are using this motor driver on a small 2 phase stepper motor with ~5mH inductance per phase.  We are having a hard time getting multiple motors to do full and 1/2 steps without decreasing step to ~ 2KHZ.  RCA/B have 47K and 1000pf; VM = 12v.  Anyone have ideas for solution?

Claud

  • Hi Claud, it sounds like you might be reaching the max RPM that you can commutate this stepper at.  Does 2kHz translate to 10 revolutions per second in this case?

    You might be able to reach faster speeds by increasing VM, or by using a different regulated current level.

    Best regards,
    RE

  • Thanks for the quick response and I'll look into your 10 rps question.  The motor is spec'd at ~4500 steps/sec.  We have no problem running at 1/4 and 1/8 step at 4400khz.  Current sense is .1 ohm.  Vref is ~ 2v.

  • Looks like we need to keep Fs, frequency start, < max F and then step our way up.  Started at 500Hz and stepped my way up to 4Khz..

    Claud

  • Yes, ramping up the speed can help due to internal resonance.

    If VREF = 2V and RISENSE = 0.1Z, the DRV8811 will regulate current to 2.5A.  Does that match what you want?  Some of the smaller steppers use much less than that.  An option you have is to see if you get better results with a larger RISENSE.

    Best regards,
    RE