I have a problem with the DRV8836EVM. When I connect a motor, the EVM supplies a max of 800mA. If I connect my motor directly to the 3V power supply, the motor draws the full 1.5A specified for my motor.
Interestingly if I combine the two halves of the HBridge together the motor still only pulls 800mA, with each half of the HBridge supplying a measured 400mA.
The voltage out on pins A1OUT A2OUT is 3V, so it seems to be a current limitation.
I'm running the EVM in "IN/IN" mode and I'm using the onboard toggle switches to control the motor.
Can someone please advise what could be causing this, and recommend some possible solutions.
Thanks in advance.