Other Parts Discussed in Thread: DRV8302, DRV8301, DRV8301-Q1
Hello E2E commuinty,
I developed a sensorless BLDC motor controller board to control the XK4082 1500KV 6cell Brushless Inrunner motor from Hobbyking using back EMF sensing, but was not able to reliably control the motor at <50RPM due to very small back EMF signals (<100mV). Our application requires a robust low speed (<20RPM), high torque (70A) sensorless BLDC controller as the motor is used in lower limb rehabilitation.
My questions are:
What is the difference between the DRV8302 Kit and DRV8301 Kit and which would you recommend?
Is there a kit for the DRV8301-Q1? Will it be more robust as it is automotive qualified?
Are encoders required? I did not think they would be as these boards are for sensorless control, but when I called the TI representative he was very adamant that encoders are needed for the DRV83xx kits to work for any motor.
Are there inputs on the kit boards for encoders?
Can encoders be used with the open source INSTASPIN-MOTION code to improve the low speed velocity control issues caused by guessing velocity based on time between commutations?
What are the breaking (stopping) capabilities with these kit boards (i.e. 1000rpm to 0rpm in 10 miliseconds)?
What are the speed reversal capabilities with these kit boards (i.e. 1000rpm to -1000rpm in 10 miliseconds)?
Thank you in advance for your help,
Aaron