Hello,
I want to build a 4-quadrant VSD to evaluate different sensor-based drive control algorithms, possibly by taking two of the DRV8312-69M-KIT, coupling the motor shafts, and connecting them to the same input bus. The issue here is that the DRV8312-69M-KIT doesn't have a motor which comes with an encoder or Hall sensors (although these inputs appear on the schematic). What I would really like is a kit that could run a Piccolo MCU and a Teknic motor shown in the 2MTR-DYNO kit, as they appear to have built-in encoders. Also, the Teknic motor is sinusoidally wound, but what about the motor in the DRV8312-69M-KIT? Could space vector control be used on both in this case?
Finally, I heard some mention in a different post of a new kit to replace the DRV8312-69M in the next few weeks. Is this true?
Thanks,
Jared