I am building a controller in Simulink for the BLDC motor (DT4260-24-055-04) of the DRV8312EVM kit.
For the simulink block of Permanent Magnet Synchronous Machine, I need to know the following parameters:
Inertia, friction factor and pole pairs [ J(kg.m^2) F(N.m.s) p() ].
I fill in these parameters with the value of [0.68e-3, 1e-3, 4 ] .
But I am not sure about if the Inertia and friction factor are correct or not.
Could anyone please check them for me.
Thank you in advance.