I refer to Fig 4 on Page 12 of the qsg_hw_hvmtr_r1p1.pdf included in Motorware 1_01_00_09 and I quote:
"Due to a contention problem with the UART connection on the board, the UART-to-Serial adapter on “–ISO” controlCARDs MUST ALWAYS be disconnected."
What does this mean and is it still true? It seems to imply that we cannot use the isolated interface on the control card with the HVkit - but other documents say we cam and should. Indeed I am doing so with the "yellow" hv board.
The same document also states on page 13:
"If you run a project from the MCU Flash you will need to remove this jumper to sever the JTAG connection and boot to flash properly"
What does this mean for our own hardware designs? If we want our own hardware to run with minimal modification from the HVkit sample code - which emulator interfaces should we support - and how do we support both running from ram and flash? I think Chris recommended using an isolated JTAG emulator from TI - and leaving isolation off our own hardware. Can you point me to an example or a specification for the JTAG header we need to implement in our own hardware that will plug directly to your isolated emulator?
My intention is to develop and test our software (as far as possible) using the HV kit prior to finalizing our hardware. Is this a realistic approach? Can CCS readily switch between the USB interface on the iso control card -and a jtag header via a JTAG isolated emulator? Can this configuration support both ram and flash operation and booting?
Thanks.
Richard.