Hi,
I am using DRV8833 IC for my application.I plan to use this IC for my satellite application .I am going to operate at the voltage of 8V.The current should flows through the load(Inductance) in one direction approximately 22.5 sec and current direction should be reversed in another direction approximately 22.5 sec.Will this IC suitable for the above application..?
Also I need some of the information I need for this part number
1. What is the maximum VDS voltage of the internal FETs.
2. Max Freq of operation if 50Khz which is indicated in datasheet, but what is the maximum duty (On Time) allowed ?
3. What is the charge pump output voltage.
4. The chip has an internal OCP, will you able to program the OCP deglitch time ?
Kindly clarify the above questions
Regards
Rajvel M