I have an application where I need to remove motor drive capability through a safety interlock. Using a digital input, such as Enable, is not acceptable. When the interlock relay is actuated, the supply (between 24 V and 32V) will decay very rapidly.
1) The clock and other inputs will still be active - will this overstress any inputs or damage the part since the internally-derived logic power will also go away?
2) When power is restored, it will rise fairly quickly. Will this damage the device?
3) Related to 2), if I hold the part in Sleep or Disabled while power is restored, will that reduce any chance for damage? Thank you!
Tony Syracuse