This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BLDC CONTROLLER

Other Parts Discussed in Thread: UC2625, DRV8312, DRV8313, DRV11873

Hi,

Our customer is looking for a controller for a BLDC motor that can provide control of the motor speed like the UC2625, but without a built in power stage. They would also like an SPI or CAN bus interface.

Is there anything from TI we could offer them?

Thanks,

Rani

  • Hi Ran

    We have a very close device which is going to be released soon. You can contact TI sales team with your projects information. Maybe it will be matched with the projects and release schedule.

    Beside, for BLDC motor driver. You can have following solution for now.

    MCU + DRV830x + MOSFETs (60V, 80A+)

    MCU + DRV8312 / 8332 (50V, 3A / 8A)

    MCU + DRV8313 (60V, 2.5A)

    DRV11873 (12V, 1.5A) sensorless and totally integrated

    Thanks.

    Wilson Zuo

    Motor Application Team