This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8301 EVM Board's DIMM100 Socket

Other Parts Discussed in Thread: DRV8301, CONTROLSUITE

Hi,

I have a DRV8301 motor control kit. I want  to design my own power stage for this kits control card .I could not find any PCB layout file for DIMM100 socket which used on this board for plug the control card.

Is there a library or layout file for this socket for any design platform.

  • Hi Furkan,

    The Allegro .brd file can be found in ControlSUITE. It is typically located at:

    C:\TI\controlSUITE\development_kits\DRV830x-HC-C2-KIT_v104\~DRV830x-HC-EVM-HWdevPkg\DRV830x_RevD_HWDevPKG\Layout  and is named DRV830x_D1-Release.brd

    I tried importing the file into Altium, and was able to obtain the DIMM100 footprint. Hopefully you can import the file into the layout program you are using.

  • Hi Furkan

    You can install controlSUITE and found the gerber files in the folder like following path on your computer.

    C:\ti\controlSUITE\development_kits\DRV830x-HC-C2-KIT_v104\~DRV830x-HC-EVM-HWdevPkg\DRV830x_RevD_HWDevPKG\Layout\DRV830x_D1-RELEASE_GERBER

    If you use protel or Altium, you can make a new CAM file then import the gerbers.

    Or you can find the part number from the BOM which should be "molex100-71251-5101".

    find as below. You can refer to the datasheet and drawings.

    http://www.digikey.com/product-detail/en/71251-5101/WM2079-ND/1989320?WT.z_cid=ref_octopart_dkc_buynow 

    Thanks.