Other Parts Discussed in Thread: HVPMSMMTR, TMDSHVMTRINSPIN, DRV8301, MOTORWARE, LVSERVOMTR, 2MTR-DYNO
I need to buy a motor for my new DRV8301-69M-kit that I just received. Can you please give me suggestions. Also, the web says that the controler is a 60 V, 60 A unit. Is this the output of the controller to the motor? I already bought the following motors for my other controller: HVACIMTR, HVBLDCMTR, and HVPMSMMTR motors for the TMDSHVMTRINSPIN controller. Will these motors work with the DRV8301-69M-kit? If not, please suggest other motors.
Thank you