This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Current input to the 8301-69M-kit

Other Parts Discussed in Thread: LVSERVOMTR, 2MTR-DYNO, BOOSTXL-DRV8301, LAUNCHXL-F28027F

Hello, I will be powering up the 8301-69M-kit soon, DRV830x Rev D. Hardware Quick Start Guide, on step 6 page 9, it says to connect 8-60V DC power supply to the PVDD and GND terminals.  But what is the input current limit?

I'm thinking of purchasing an AC/DC converter that will plug in the wall (120 VAC), to generate the V DC power for the kit, but i need to know the current input.

  • Hi Michael,

    The amount of current required will depend on the type of load. Without any load on the half bridges the board will not consume more than a few 100mA. The board supports ~40A max.

  • Does TI sell any motors for the 8301-69M-kit?  AC Induction or PMM? since it's 60V, 60 A output. 

  • Michael,

    Our standard motor for this kit is the LVSERVOMTR.  You can run this motor to 50V+ and it will pull over 7A.

    You can also purchase two of these with coupling and frame mount as 2MTR-DYNO

    We will soon offer a LVACIMTR that will also couple/mount into the Dyno as well.

     

    Technicaly, none of these motors are really ideal for the 66V / +/-40A scaling.  The LVSERVOMTR works fine for demonstration and education on this board (though their low speed performance suffers). It is important for best performance to scale your HW voltage/current to the motor you are using to maximize resolution.  We do not offer a low voltage, high current motor for this board....a motor like this is typicaly found in a power tool, automotive pump, or an e-Bike.  These motors are a bit better suited.

    We also have the BOOSTXL-DRV8301, an inverter designed for 6-24V/10A.  Better scaling for these lower voltage/current motors.  Currently this uses a LAUNCHXL-F28027F for control, running InstaSPIN-FOC examples.  We are also working on another LaunchPad with more features :)

    Good Luck!