This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Best solution to isolate LMD18245 from uController

Other Parts Discussed in Thread: LMD18245, DCH010505S, REF02

Hi,

I'm planning to use LMD18245 to drive a Bipolar Stepper Motor (24V 1.8A 1.8°) with microstepping (quarter step drive with torque compensation).

Schematic that I plan to use is the same on datasheet

Below the functional block diagram reported for convenience

I have some question:

- What is the best solution to isolate Motor and Driver from micro controller? I am thinking using optocoupler with LMD18245 input but so I've to genere DAC REF from motor power supply that can be noisy when motor are running. There are better way?

- How can I use external DAC? There is only CS OUT and COMP OUT input, I need also an external comparator?

Thank you

Leonardo