Hello, I have a BLDC motor, that operates at 48Vdc, and I've already purchase 3 DRV8332 and a Piccollo C2000 Launchpad for developing a motor controller requested for an Eco car contest.
Problem is I believe the battery from this hub motor has a continuous dicharge Current of 20A and holds current peaks of 50A, but I'm afraid that I can't even make the motor to start with the DRV8332 before it triggers its OC security turn off.
http://www.goldenmotor.com/e-Bike-DIY/MP3%20SmartPie%20Wiring%20Layout.jpg
The motor works between: 20-48Vdc
has a power rate of: 250W - 1000W
Is there a way to use this DRV8332 or should I abort the mission and use mosfets?