Hello, I just received the 2MTR-DYNO kit from TI, I have the DRV8301-69M-KIT. Currently, I need to connect one of the motors to the 8301-69M-KIT. The motor has the 16-pin Molex, was i suppose to receive the mating connector to the kit to connect one of the motors to the kit? none was included in the package, I thought TI would include the mating cable to go from the 16-pin molex from the motor to the connectors on the 69M-kit. What is the part number for the mating cables so I can buy two of them for both motors.
There was no documentation included in the 2MTR-DYNO box. Can I run some of the labs in the instaSPIN projects and Lab User's Guide?