Hi,
i want FULL Bridge driver IC same as SM72295, but its VCC should be 20v or more.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Vinay,
The closest DRV device we have is the DRV8711. It can drive 2 external H-bridges and supports 52V VCC.
Does it need to be a pre-driver? What kind of current does your application demand?
Hi Nick,
i already designed a charge controller board with SM72295, but it had the vcc of 14v but i want it more mean 20v or above.
so i need same 28 pin package model. please lemma know if any IC is there.
Thanks and Regards
Pavan
Hi Pavan,
I don't believe we have a drop in part for a higher voltage at this moment.
Hi Pavan,
Yes, Nick is right, we don't have a higher Vcc drop in compatible part for the SM72295.
Why is there a need for a higher Vcc?
Thanks,
Shashank