This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FOC control PWM setup in DRV8301LS12 Evaluation kit



Hi,

I am using DRV8301LS12 evaluation kit. 

When  I look the sample code for FOC comes along with the kit.

They have implemented 20KHz PWM and PWM TBCLOCK is 80MHz.

In PWM period register, instead of 4000/2 (half period value as UPdown counter mode is used),  its entered with value(3900/2).

Is there any specific reason for this implementation?

Thanks & Regards,

Rathinavel