We are have problem with drv8432 VREF goes low without any motion or motor connection
We replace a digital [pot and we put AGND a 64.9K resistor , also we added a 4.3K pull down resistor to RESET_AB and RESET_CD pin.
The problem appear when we run the software trough a JTAG port , the DSP IO's are 3.3. V
We are facing this problem recently and we are close to be in production ,
What can be the problem that VREF goes low , , we are using a LAB power supply with protections, guarantied w no over current happen, We are in the dark here with this problem
Second Question: when Vref goes low means drv8432 burned ?
Albert