Hi,
I'd like to ask about "OCP time" in DRV8842 datasheet (page 10, section "Overcurrent Protection").
Could you give me the value of this time? In best case a MIN, TYP und MAX value.
I couldn't find it in the datasheet.
Regards,
Sebastian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I don't have the MIN/MAX data, but a reasonable estimate is ±20%. Do you need to know precisely?
Best regards,
RE
Sebastian, I found our digital logic specification, and it provides a ±10% range for the time.
Best regards,
RE
Sebastian, sorry but today I found what I told you is incorrect. I received new info from the device designer. The OCP deglitch time is typically 3.0us, and there is also roughly 400ns of propagation delay. So you can expect about 3.4us between overcurrent and when the device trips the fault.
Best regards,
RE