Is the input/trigger pin on the DRV2605 tristate?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is the input/trigger pin on the DRV2605 tristate?
Hi, Jacob:
NO.
the input resistive impedance is about 100KOhm.
if not used, this pin can be grounded or float.