can someone help me with the internal waveform memory of the drv2667. i
would like to save and play rectangular waveforms, ramps, etc..
however, the example from the datasheet shows only how to store the given frequencies in the internal memory.
or is it not possible to store waveforms that are not sinusoidal?
ps: i dont wanna use the fifo, and analog in, because i have multiple drivers which should play the waveform at the same time or at different times, and the waveform is only started from the microcontroller