I am using the DRV8301-LS31-KIT with the supplied motor.
I am trying to control multiple H-Bridges with DRV8301 chip. I added wires to the GH and GL lines on the PCB. When I connect one GH and GL line to my additional H-Bridge circuit PCB, I get a Fault indication which I believe is an OC fault. My additional board uses a battery for a supply so it is isolated from the main board DC power supply. The sense lines SH_ and SL_ are only connected on the main board.
I want to change the OC_MODE (as stated in TI app note SLVA552) to D4=0 & D5=1 for report only.
Using CCS, which file does this control register reside?
Thanks
Alan