This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Stepper Motor Driver replacement for DRV8255

Other Parts Discussed in Thread: DRV8825, DRV8829, DRV8711

Hello,

Currently we are using DRV8825 driver to drive 1.7 A Stepper Motor.

To increase the performance, we are planning to use 2.5A Stepper Motor / 2.55V

Are there any drop-in replacement driver

or

can you suggest us the driver that can provide all the functionality of DRV8825 plus higher current.

Please let us know, if you need any further information

Thanks.