This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8307 Can handle Max RPM question

Other Parts Discussed in Thread: DRV8307

DRV8307 can handle BLDC max PRM by different motor question ,

By 4-pole BLDC max PRM is ?  (can handle over 20000 RPM ?)

By 8-pole BLDC max PRM is ?

  • Hi James

    RPM = FG*60/(POLE/2)

    FG limit for DRV8307 is 6.7kHz

    So, you can get RPM = 200000 for 4pole and 100000 for 8pole motor.

    That is a very high speed which is close to the limit of most BLDC motors. DRV8307 is good at driving fast motors.

    Best regards

  • Hi James,

    The max operating Hall input frequency is 30kHz.  For a 4-pole BLDC, that equals 900k RPM.  For an 8-pole BLDC, that equals 450k RPM.

    I think usually the motor used and VM voltage will determine the max RPM.

    Best regards,
    RE