I would like use a application with forward DC/DC conversion like in DRM078 from freescale ( bldc-Motor has L about 60uH only).
I want to disable the overcurrent-functionality (page 14:ConnectOC_ADJ pin to DVDD to disable the over-current protection feature.)
And connect on Pin PVDD1-29 wired-OR of 10V-supply and output of DC/DC-convertor for motor-voltage.
see in 3-Phase BLDC Drive Using Variable DC Link Six-Step Inverter , Designer Reference Manual, DRM078 Rev. 1 05/2006- freescale, page 12:
It is correct? Will it good work?
Zbyno