This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8841 and DRV8843 Full Torque function at Half Step driving

Other Parts Discussed in Thread: DRV8843, DRV8841

Hi

My customer is considering the motor driver, they're the candidate of ON-Semi LV8702V.
LV8702V: http://www.onsemi.jp/pub_link/Collateral/ENA2121-D.PDF

They need Full Torque at Half Step driving as most important function.
->Indexer logic control the current '100%=>71%',
    It's not much to customer request.They need '100%=>100%'.

I would like to recommend DRV8841 and DRV8843 for this business.
Can DRV8841 and DRV8843 support the Full Torque?

Best regards
Shimizu