.
I am trialling a DRV8308EVM to run a Papst ECA 18.08 http://www.ebmpapst.com/en/products/motors/ecigearmotors/ecigearmotorsdetail.php?pID=54331
With the motor not loaded or driving anything, I can get a good lock with minimum flutter. I am using 180 degree sine-wave and the motor frequency is 234Hz. MOD 3970 and XOR the sensors.
The problem arises in the intend application, where the motor has to run at 234Hz and is driving a flywheel 12" diameter that weighs over 4Kg. It is run through a small pulley on the motor to a flange on the flywheel via a rubber belt to give an actual speed of 33 1/3 RPM.
So in essence, it's a small motor going slowly, driving a big flywheel going extremely slowly, coupled by a small rubber belt.
After two whole days I cannot get lock, only approximate speed stability with a huge amount of flutter ! I don't need phase lock, but I do need a fairly tight frequency lock.
I am looking for a solution using this or any other device. This is not for a 1 off so it needs to be a manufacturable solution and work totally reliably in the field. Free help would be great, or if I have to, I'll pay someone to do it ? motor@time-step.com
Thoughts please ?
Thanks
Dave