From the website it looks like DRV8834 and DRV8846 have eval boards. I would like some help in deciphering some of the information. For example, the DRV8834 eval board user’s guide discusses motion control and setting the start speed and target speed in PPS (pulses per second or full steps per second). It identifies a minimum allowed of 200 PPS. Based on the motor that we would be driving, I believe the minimum would be a problem. Is this software-limited on the eval board or hardware limited in the DRV8834? From what I can tell, the motor with speed of 200 degrees per second, would be equivalent to 11.1 steps per second (200 deg/sec divided by 18 deg/step). Based on the definition of PPS, this is less than the minimum allowed 200 PPS.
Am I reading all this correctly? Based on the motor we are trying to drive, what does TI recommend as the best fit? Here is a link to the motor: http://bit.ly/1lD0c6m