Hello,
We are planing to use DRV8711 drivers with TivaC uCs. But I need some answers before schema.
1) Do I need to isolate Power Line of Microcontroller and DRV8711 from each other with an Isolator. (Seperated Grounds?)
2) Do i need Digital Signal Isolating for Step,DIR and Communication Lines?
3)I have DRV8711EVM and I ve seen there is nothing to isolate. This can be trustable?
4) Can i use Regulated 5V from DRV8711 5VOut pin to supply TivaC(Sure after regulating it 3.3)