Hi TI Engineers,
I am interested in using the DRV8301 as a pre-driver to power a BLDC motor. I would need to achieve similar functionality to what is possible on the BOOSTXL-DRV8301, specifically the 10 A output current.
From what I could find, the only IC that could achieve such a high output current is the DRV8332. However, I assumed that if I could take the discrete components from the booster pack with the 8301 and add them onto my own PCB, then I could somehow replicate the high current output. (this is necessary because I plan to mount this on a RC plane to control the BLDC motor).
Can anyone shed any light on if the DRV8301 can be used to get this output?
Much Thanks,
Aleksandar Zivkovic