I am looking to use the DRV8850 in my new design and I had a few questions which are a bit unclear from the datasheet:
1) Once VCC falls below the LDOOUT Voltage (set by the feedback resistors), what is the LDOOUT voltage?
2) It seems that ~40 uA (I_VCQ2) is consumed with just the LDO on and motor driver off. When the input voltage falls below the LDOOUT voltage (set by the feedback resistors), does the chip still consume this current?
Thanks.