I hope to drive stepper motor with direct pwm input mode to get my own micro-step resolution.
(1) Is it possible to drive stepper motor with the direct pwm mode?
(2) Is it possible to add additional OPAMP for monitoring current on shunt resister ?
(3) When using the direct pwm mode, I wonder to kown the operation of auto mixed decay function.
Thanks.