I have a nice DRV8301 BOOST board here and I'm trying to chase down a problem.
Right now, I don't have the SPI running on my prototype board. I'm seeing the PWMs running but there's no voltage out from the board, and none of the fault lines are active.
I have EN_GATE hooked to the 3.3V giving it s solid HIGH.
I'm assuming that, by default, when the chip powers up I can just feed it with the PWMs and I should see something come out, right?
All help appreciated.
Ed Averill