This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8818 Shutting Down

Other Parts Discussed in Thread: DRV8818

I am starting the development of a board using the DRV8818 stepper controller however it keeps shutting down the output drivers.  I am not entirely sure why this is happening as I don't believe that any short circuits / over current or over temperature protection is kicking in.


The stepper motors I am using are rated at 0.8A 12V with a measured winding resistance of 16 ohms.  I have verified that there are no short circuits between the motor phases (measures resistances between A+/A-/B+/B- while connected to the driver).


When I apply power to the driver (with no pulse inputs) power is applied to the motor for approx 15 seconds then the DRV8818 drivers seem to turn off.  When power is applied I can not turn the shaft (as expected).

If I apply a step signal to the driver it seems to disconnect the output drivers immediately (1-2 seconds).


To verify that I am not having any over current issues I have inserted a 10 ohm resistor in series with the 24V power supply I am using.  This will limit the maximum current to the DRV8818 to about 2.4A.  With this resistor in place I am still having the same issues (its not possible to have an over current lockout in this case, right?).  The average voltage across this resistor is 5.3V (530mA).

I can also touch the the DRV8818 chip and it still feels cold so thermal lockout is also not likely.
Do you have any idea what could be causing the output drivers to shut down?

I should also mention that I might have a poor board (grounding) layout as the voltage across my 0.20 ohm sense resistors seems to have about 50mV peak to peak noise present.  At the full motor current of 0.8A it should be 160mA, so the only issue I can see this causing is that the noise might be limiting the current to a lower value than the 0.8A I set it to drive.


Edit: I should note that I am sending the control signals to the driver from a micro controller powered from the same 3.3V supply as the driver.

  • Stoudt,

    As per my understanding device can trip due to followings:

    1. Logic state change at Enablen/Resetn & sleepn: check-out that all these input logics are proper state to keep the device in active mode.

    2. Under-voltage lock-out  at VM and VCC: Check this out. Btw your method to confirm about over-current protection by inserting 10ohm resistor in series with 24VM is not that appropriate. Some-time during transeint conditions if high current is drawn from Vcc, it may cuase unver-voltage lock-out.

    To confirm that it is not over-current, I would suugest to add this resistor in series with motor winding at output. This will make sure that you never hit over-current even if motor winding resisance comes down.

    3. Also check that power-pad beneath the IC is properly soldered to GND plane on PCB.

    Best Regards

    Milan-Motor Application Team