HEllo,
I am trying to connect the DRV8802 EVM to my Windows XP system.
I have followed all the instructions from the "readme" pdf .
I have changed to COM port settings and chosen "COM port 3" for communication.
However, I do not see the pin toggling reflecting on hardware. Any changes that I do in the GUI are not reflected on the EVM.
The GUI says "connected" and the text box has turned green .But I dont think that it is communicating with the EVM.
Also the Status LED on the EVM is off.