Hello,
The stall current varies from 1.2A(min) 1.86 (typ) and 2.1A (max) .
The Over current for DRV8802 is 1.8A to 5A.
300mA is the preprogrammed load current.
So here is my understanding -
1.2A - This vaule is lesser than over current limit but greater than 300mA. So the device will try to regulate the current to 300mA .
Question: For how long does the regulation take place?What will be the final value of current - 300mA or 1.2A ?.nFault will not be driven low ?
1.86A and 2.1A : This value is greater than over current limit .The FET is disabled and nFault will be driven low (after blanking time which I learnt 3.75uS ).
Is this understanding on track ?