I had a DRV10983 EVM successfully operating with the supplied Runtian BLDC motor with a 24V supply. I then attempted testing our application motor (BLDC, 1.6A max, 24V) with the EVM but the DRV10983 iimmediately smoked when the 24V supply was connected using the same order of connection as specified in the EVM quick start guide. I don't believe that there were any incorrect connections.
I have replaced the DRV10983 and the EVM is working again with the Runtian motor at 24V. Before I potentially create more damage is there anything different that I should be doing before testing this alternate motor?
Appreciate any inputs.