I have a launchpad with a MSP430G2553 and I have attached the Boost-DRV8711 Eval kit to it. I believe I got the MSP430G2553 flashed correctly and I have the GUI for the Boost-DRV8711 Eval kit up and running with no error codes. However, I am unable to get my motor to run. I see that my nFAULT and nSTALL are both high according to the GUI and from manually checking the board with a meter. I am also able to set the RESET high with the GUI and I can see that it is set high on the board by checking it with a meter. However, when I set nSLEEP high and check the board with a meter, the nSLEEP pin is low and not changing. Is there something wrong with the board or am I doing something wrong?