This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

encoder connection to dsp

please i have some questions about encoder and using it with DSP. I know that there is a type of encoder gives three signals (A, B, and Z)  (quadruture )and this type can be used with the eZdsp 28335 but when i went to the motor company, i found only motors with a built-in type of encoder gives (T+ and T-  signals) (as the seller said)  dn't know this type and i  dont know if thiis type can be used with the dsp or not and how can i use it

i will use it to measure the speed and   initial postion of PMSM