I intend to use your 2MTR-DYNO to begin my starting tests. After a great deal of research, one LAUNCHXL-F28069M with two BOOSTxl-DRV8301 is the ideal setup for the dyno system mentioned above.
After that I would like the option to change the motors to a BLDC motor similar in size to those use today in small UAV aircraft. This "motor" will have a max voltage of 24V and max current around 40-60A. I do have freedom to vary the motor but it will definitely draw more than 10A which is the limit of BOOSTxl-DRV8301. I found that the DRV8301-69M-KIT covers most of the range I would need, however it only controls one motor.
So can I run a load motor and test motor at those powers with your Drivers/ software? Would I need two DRV8301-69M-KIT? can I use a different Booster with LAUNCHXL-F28069M to increase its current limit?
And since I am comparing, Can both of the drivers change the output waveform? (sinewave, trapezoid wave, block wave)
Thank you,
Clayton