This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Command update rate for LM629 using 4Mhz crystal?

Other Parts Discussed in Thread: LM629

Hello,

I want to inquire command update rate for LM629, using 4Mhz crystal?

Section 5.6.2 of document "AN-706 LM628/629, SNOA184D–October 1993–Revised May 2013"; states for 8Mhz/6Mhz crystal frequencies:

5.6.2 Command Update Rate
If an LM628/629 is updated too frequently by the host it will not keep up with the commands given. The
LM628/629 aborts the current trajectory calculation when it receives a new STT command, resulting in the
output staying at the value of the previous sample. For this reason it is recommended that trajectory is not
updated at a greater rate than once every 10 ms.

Thank you,

A. Zaheer