This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Two DRV8842 burnt. Running out of ideas.

Other Parts Discussed in Thread: DRV8842

Hi. I'm trying to control a 24V DC motor using DRV8842.

First I tried a quick prototyping hack, and managed to drive the motor for a while, but then the DRV8842 suddenly burned.

So I tried to make a better prototype with a custom made PCB. I connected everything (except power pad) as in the datasheet.

First I tried without any load. I don't use PWM. I got 0V, +24V or -24V on the output pins, just as expected.

Then I attached the motor. The motor did not move and the fault-LED lit up from time to time. I found that there was a mechanical problem with the motor and fixed that. I then tried to run the motor connecting 0V and 24V to it directly. It worked as expected.

Finally I tried to run the motor once again using my prototype board. During a second or two the motor ran at a very slow speed, and then the DRV8842 burned once again!

I'm not sure how to continue from here.

I'm aware that I should have the power pad connected, but since the board is hand soldered that is not easily done. And I would have thought the circuit would survive for a bit longer than a second or two?

Also, the device should shut down both by high current and high temperature.

Here's a photo of the board:

Here's the schema and board layout:

Any hints appreciated!