This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We afraid that sometimes & somehow the driver can damage the motor, maybe at wrong configuration or operation.
Is there any case that the driver can self PWM out ?
Maybe can self wake up & PWM out ?
Attached schematic screen-capture :
Motor VDD = Battery voltage = 7.4v nominal
Input PWM directly from MCU
Output PWM directly to motor
R101 isn't assembled
See inserted questin:
Is there a specific concern about how the motor would be damaged?
Yes, I'm afraid that sometimes & somehow the driver enters to undefined state & drives current to the motor
Yes there may be cases based on the schematic shown. Depending on the resistance of the motor and the Vtrip voltage, there could be as much as 6A during startup or stall. What is the motor rating?
Which case ? can you please be more specific ? it is very important, try to think if & how it can happen. attached motor's datasheet
The DRV8833 regulates current in the motor based on the value of Isense. When used in parallel mode as shown, you can achieve up to 4A assuming thermals are met, and possibly higher if the Isense is set above 4A.
As you can see we set the overcurrent protection to 5A, the motor isn't able to pull this current
Hi Eli,
eli said:Is there a specific concern about how the motor would be damaged?
Yes, I'm afraid that sometimes & somehow the driver enters to undefined state & drives current to the motor
Yes there may be cases based on the schematic shown. Depending on the resistance of the motor and the Vtrip voltage, there could be as much as 6A during startup or stall. What is the motor rating?
Which case ? can you please be more specific ? it is very important, try to think if & how it can happen. attached motor's datasheet
Thank you for the motor specs. The case when the motor stalls, and becomes a resistor. In some cases the voltage is higher than the motor manufacturers rated current and can cause the motor to overheat. This does not appear to be the case for this motor.
When the motor stalls, the current will be limited to approximately 4A. At some point this will cause a thermal shutdown and the nFAULT pin will assert. Monitoring the nFAULT pin provides feedback of potential problems like the overtemp or overcurrent.
With regards to the device self waking, we have not heard of any issue like this.
Hi Rick
Is there any SW recommendation for operating the DRV8833 with MCU (PWM, Freq, Delays etc') ?
I have noticed that revision c of datasheet is released
Why In this revision the feature "1.5A RMS, 2A peak" defined only for RTY package, while previous datasheet version it was defined in PWP & RTY packages ?
Can you please advise for advantages and\or disadvantages between the two packages RTY & PWP (price, electrical & thermal conditions & ratings)
Hi Eli
The thermal performance of RTY is very similar or a little better than PWP package. 3A RMS/ 4A Peak should be fine for both the RTY and PWP package. RTY just saves your PCB room. For high current application, the PowerPAD of RTY package is also or more needed to have very good connection to large copper for the dissipation.
Best regards,