Hi,
I am considering the following configuration.
① Brushed DC motor 3channels and relay driver 2ch for solenoid drive.
②Brushed DC motor 4channels and relay driver 2ch for solenoid drive.
I think that DRV8823 is best for the case ②.
For ①, will not be able to use the DRV8823?
And give away the remaining H-bridge 1 channel, and lodge as an independent FET, I'm glad to be able to reduce one the IC.
I can consider another use if used as one of the FET.
However, if it is used as a relay driver, I would like to the PWM control of several hundred Hz.
Please tell me whether this method is possible.
Thanks.