I connected the DRV10983 board to USBANY and spent some time tuning it with a HDD Spindle motor.
No matter how I tried I could get the speed beyong 1400rpm. At 12V, the no load current was 0.6A.
Something I missed or any recommendations?
Thank You
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I connected the DRV10983 board to USBANY and spent some time tuning it with a HDD Spindle motor.
No matter how I tried I could get the speed beyong 1400rpm. At 12V, the no load current was 0.6A.
Something I missed or any recommendations?
Thank You
Hello,
Can you help with below data.
1. Motor resistance phase to center tap
2. Velocity constant; V/Hz
3. Rated voltage sped of motor and rated speed and rated current at this voltage
4. Number of pole
5. DRV10983 GUI basic & advance page setting, chosen by you
Best Regards
Milan
Hello,
Can you clarify about velocity constant units? 130V/Hz means to run motor 1Hz ~15rpm , 130V is required, this does not make any sense. Also, if I assume it as 0.130V/Hz, means at 12V motor will reach at 92.3Hz ~1384rpm only.
Best Regards
Milan- Motor Application Team