Hello,
Please answer following question from customer.
They want to confirm if DRV3201-Q1 can be used for DC motor H-bridge pre-driver.
(Because they want to use same PC board for DC motor and 3 Phase Motor application using DRV3201-Q1.)
They need to use “Drain Source Voltage Monitoring function”.
Please advise how can we use DRV3201-Q1 for DC motor H-bridge pre-driver.
Best Regards.