I am testing the DRV8835 using a resistive 1.4 Ohm load. Vcc = 3.3V. The schematic is the same as in figure 1 on the datasheets. The chip shut down when Vm approaches 1V with load current =500mA. I don't have an explanation for this. The chip is rated at 1.5A/bridge, so should handle 3A per figure 1.
The chip is cool, so it can't be a thermal shutdown.
Help please ?