Hello,
I'm planning to use DRV8312 for BLDC motor application. Driver will work with various motors from 12 - 48V and max constant current 2.5A. Inrush current could be up to 10x higher then normal current 25A. Additionality one motor 12V has normal current of 3.41A and starting current 29.8A.
Inrush duration is aprox 10ms.
I would like to set OVC to 11-12A. Will DRV8312 work (in CBC mode) with 25A of inrush current 10ms? Is it possible also to work with 29.8A inrush to for 12V motor? How will motor startup looks like if DRV8312 works in CBC mode?
Motor spec
Thanks,
Janusz